cancel
Showing results for 
Search instead for 
Did you mean: 

main specifics of LSM6DSOX

amuel.1
Associate II

Hi together,

I am new to the topic mems and got some difficulties in evaluation by reading datasheets.

Many datasheets include Allan Variance plots, bias instability, misaligment and etc..

I couldnĀ“t find those parameters in documents of LSM6DSOX.

I want to callculate velocity and position by using accelerometer and gyroscope.

I thought random walk (which is mentioned in the datahseet as "Rate noise density" I guess ) and bias instability are one of the most influental parameters in relation getting a "more" accurate velocity and position.

Which are the parameters I have to consider for achieving accuracy in velocity and position as good as possible?

Thanks in advance!!

2 REPLIES 2
Eleon BORLINI
ST Employee

Hi @amuel.1ā€‹ , the datasheet parameters are the (typically) tested ones at production level. The AVAR plot (and related parameters), and the misalignment-related specs are tested at bench / lab level. I could share you typical characterization data for the AVAR parameters, and a typical plot for the 6 axis.

0693W000000WG4XQAW.png

where ARW = angle random walk, BI = bias instability, RRW = rate random walk.

Here below the AVAR plots for the DSOX device (1st picture for accelerometer, 2ndpicture for the gyro part):

0693W000000WGXUQA4.png0693W000000WGXeQAO.png

Regards

amuel.1
Associate II

Thanks a lot for your help!!