cancel
Showing results for 
Search instead for 
Did you mean: 

LSM6DSV16X FIFO batch data rate

fluchc
Associate

In high-accuracy ODR mode, can the frequency of writing to the fifo be automatically aligned,

for example 960 to 1000hz

fluchc_0-1724837138350.png

fluchc_1-1724837142546.png

 

 

1 ACCEPTED SOLUTION

Accepted Solutions
Federica Bossi
ST Employee

Hi @fluchc ,

The FIFO rate is always aligned to the ODR or its submultiples. If you put 1000 Hz and BATCH_RATE = 960 Hz then BATCH_RATE will also be 1000 Hz. If for example ODR = 1000 Hz and BATCH_RATE is 480 Hz then the real batch_rate is 500 Hz.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
Federica Bossi
ST Employee

Hi @fluchc ,

The FIFO rate is always aligned to the ODR or its submultiples. If you put 1000 Hz and BATCH_RATE = 960 Hz then BATCH_RATE will also be 1000 Hz. If for example ODR = 1000 Hz and BATCH_RATE is 480 Hz then the real batch_rate is 500 Hz.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

thanks