2023-11-22 12:29 AM
I used the lsm6dso32x_read_data_polling example and got the same result as above.(with SPI)
Is this the correct value?
And when I checked the values using Unico GUI tool, I got the same values as above.
Although the values are similar to the example, they are slightly different. So I'm a little confused. Is this okay?
Thank you.
Solved! Go to Solution.
2023-11-22 1:43 AM
Hi @sygo ,
Your data seem ok, I don't know in which position you had the sensor but they make sense.
The little difference between the two measurements can be due to little movements between the first and the second one.
2023-11-22 1:43 AM
Hi @sygo ,
Your data seem ok, I don't know in which position you had the sensor but they make sense.
The little difference between the two measurements can be due to little movements between the first and the second one.
2023-11-23 12:19 AM - edited 2023-11-23 12:24 AM
Hi, Federica Bossi
Thank you for your answer.
And I have one more question
An5629 Datasheet Section 8 FSM Configuration Example implemented only Accelerometer.
I don't understand.
It seems that you did not set what data you use with FSM, but I don't understand how it was used as an Accelerometer.
How can you tell me how to use it as an Accelerometer?
Also, Can you tell me specifically how to create the Threshold? I don't quite understand.
2023-11-23 7:01 AM
Hi @sygo ,
Can you open a specific topic for this question? so that if other users have the same doubt they can find an answer more easily. I also ask you to select the answer to your previous question as accepted solution. Thank you!
As soon as you create the new question I will answer it :)