2024-11-27 10:56 AM - last edited on 2024-11-27 11:30 PM by Peter BENSCH
Hello!
First I would like to state my issue:
1. My software cannot connect to the LSM6DSO IMU sensor.
A little background on my project is that I am trying to use the IMU sensor to provide accelerometer readings in x, y, and z directions. I purchased a breakout board from Sparkfun that uses the LSM6DSO to test the sensor first with my Arduino-compatible controller via SPI communication. This proved that it works.
We then created our own design and referenced the way Sparkfun wired the LSM6DSO. Now when I run the program on the new board, the sensor doesn't work.
I looked into the library that Sparkfun uses for programming in Arduino and I see that it cannot connect to the IMU sensor. In the library I can see where it fails and it fails when checking the part ID. I keep getting a part ID of 255 which is 0xFF. I should be getting a part ID of 108 or 0x6C.
Any ideas on what I can do to make it work?
uint8_t partID;
readRegister(&partID, WHO_AM_I_REG);
if( partID != 0x6C ){
Serial.println(partID);
return IMU_HW_ERROR;
}
else{
Serial.println(partID);
return IMU_SUCCESS;
}
2024-11-27 11:59 AM
I had a Bluetooth module that snapped into our PCB and thought it was a good idea to snap it off and only debug the IMU sensor. After I snapped it off, I am now getting a part ID of 0. Also the MISO line before didn't have a signal, now it does but still wrong part ID read. Therefore, I still get nothing for the accelerometer reading of the sensor.