cancel
Showing results for 
Search instead for 
Did you mean: 

LSM6DSO pedometer threshold/offset settings

CQuin.1
Associate II

I have one axis on the LSM6DSO that gives a lot of false positives due to some vibrations on the board. I know there is a way to set the step count and duration thresholds, but is there a way to adjust the sensitivity or motion threshold of just one axis for a constant vibration source?

1 REPLY 1
Eleon BORLINI
ST Employee

Hi @CQuin.1​ ,

please check if this thread on similar topic can be of any help for you.

You can start from checking your code with the lsm6dso_pedometer.c file on Github that configures the LSM6DSO to enable the pedometer embedded function.

-Eleon