2023-11-16 10:20 AM
Hello everyone, I am in the development phase of a wearbale project including the use of LSM6DSO and LIS2MDL sensors.
I found in the datasheets the power consumption related to the two sensors whne powered up at 1.8 V but I didn't find anythong about their current consumption on other VDD.
Is there a resuming table that links the sensor's current consumption to their power supply?
Thank you!
Lorenzo
Solved! Go to Solution.
2023-11-17 02:58 AM
Hi @LorenzoBarbieri ,
We provide the typical values only at 1.8V because the current consumption at other Vdd is tested only in characterization and thus not guaranteed in production.
2023-11-17 02:58 AM
Hi @LorenzoBarbieri ,
We provide the typical values only at 1.8V because the current consumption at other Vdd is tested only in characterization and thus not guaranteed in production.
2023-11-17 04:40 AM
Hi Federica,
thank you for the answer. I did some tests on a breakout evaluation board of LSM6DSO and found out that current consumption increases with VDD (as expected), since the project I am working on is battery based, I would power the sensors at 1.8 VDD to reach the lowest power consumption.