Question
LSM6DSL: Using inactivity interrupt without the auto-decrease of the sample rate
Posted on June 05, 2017 at 18:20
Hi,
I am using the LSM6DSL with a SMT32L476. My question is in relation to the Sleep/inactivity interrupt.
I am able to use the LSM6DSL in both sleep and wake up interruption.
However is it possible to use this interrupt (Sleep/inactivity) and disable the automatic decrease of the accelerometer sampling rate to 13 Hz option.
I tried to set TAP_CFG (58h) to 0x80 (INACT_EN = b00) but the interrupts are not generated anymore.
Can someone please tell me if it is possible and if it is how to ?
Thanks,
#lsm6dsl #inactivity ##interrupt