lsm6dsl int1
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-01-10 2:10 AM
Dear Sir.
I work with LSM6DSL with SPI bus ,
The wiring are OK , I can read the register who_am_i.
I can't makie the INT1 to work.
Attached a code
int32_t lsm6dsl_orienation_config(void)
{
int32_t ret = true;
unsigned char z;
// lsm6dsl_gy_full_scale_set(LSM6DSL_2g);
z = 0x60;
lsm6dsl_write_reg(LSM6DSL_CTRL1_XL, (uint8_t*)&z, 2);
/* Enable Interrupts TAP_CFG */
z = 0x80;
lsm6dsl_write_reg(LSM6DSL_TAP_CFG , (uint8_t*)&z, 2);
// /* Enable 6D threshold. TAP_THS_6D */
z = 0x50; //50 deg.
lsm6dsl_write_reg(LSM6DSL_TAP_THS_6D , (uint8_t*)&z, 2);
// /* Enable LP2F filter. CTRL8_XL */
z = 0x01;
lsm6dsl_write_reg(LSM6DSL_CTRL8_XL , (uint8_t*)&z, 2);
// /* 6D interrupt driver on Int1 */
z = 0x04;
lsm6dsl_write_reg(LSM6DSL_MD1_CFG , (uint8_t*)&z, 2);
return ret;
}
Please Advise
- Labels:
-
INEMO-Inertial Modules
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-01-11 8:13 AM
Hi @Community member ,
The procedure looks overall ok, according to the AN5040 application note p.40...
Please note however that this line:
/* Enable 6D threshold. TAP_THS_6D */
z = 0x50; //50 deg.
lsm6dsl_write_reg(LSM6DSL_TAP_THS_6D , (uint8_t*)&z, 2);
is writing a value out of range, since you should write 0x60 to have the 50deg threshold (b01100000).
Check also D6D_SRC (1Dh) register (datasheet p. 71) if you are still facing issues.
I suggest you to also check the lsm6dsm_orientation.c sample C code for the interrupt management.
Please note also that the name of your function is "orienation", in case you are facing misspelling issues.
-Eleon