2019-01-03 6:40 AM
Dear All,
I have several questions regarding the absolute maximum acceleration, which the chip (LSM6DS3) can resist. The Datasheet says it is 10000g for 0.2 ms
My questions are:
* Is there any difference if the chip is powered or unpowered?
* What does the value exactly mean? Is it valid for the sum of the accelerations, e.g. if you have 8000 g on X and 8000 g on Y it is above? Or for every axis separate, so you can have a 8000 g on X and 8000 g on Y?
* What can be the expected result if the chip is exposed to more than maximum, should it stop returning data or will give incorrect values?
* Maximum range is 16 g, I suspect that everything above that will just be returned as 16 g acceleration?
It will be very helpful you have and can share this information as the device, on which I work may accidentally fall from height and we it should survive this fall.
Kind Regards,
Stanislav
Solved! Go to Solution.
2019-01-06 4:23 AM
2019-01-06 4:23 AM
2019-01-07 8:47 AM
Thanks a lot for the answer!