2020-10-29 06:22 AM
Hi. What are the differences between them?
Solved! Go to Solution.
2020-10-30 03:13 AM
Hi @Bacteriusartnik ,
ok I just see you have edited the post.
LSM303AH and ISM303DAC are very similar chip: the main difference is that the ISM303DAC ha been qualified in industrial conditions, while the LSM303AH ins standard conditions.
If your application is not industrial, you can use the LSM303AH.
-Eleon
2020-10-29 08:43 AM
Hi @Bacteriusartnik ,
are you referring to the LSM303DLH, right?
The ISM303DAC device has in general better performances than LSM303DLH one, especially regarding:
-Eleon
2020-10-29 09:06 AM
Hi im referring to: https://www.st.com/resource/en/datasheet/lsm303ah.pdf
2020-10-30 03:13 AM
Hi @Bacteriusartnik ,
ok I just see you have edited the post.
LSM303AH and ISM303DAC are very similar chip: the main difference is that the ISM303DAC ha been qualified in industrial conditions, while the LSM303AH ins standard conditions.
If your application is not industrial, you can use the LSM303AH.
-Eleon
2022-05-06 04:56 AM
Hi,
I have a related question: Can we use ISM303 for Tilt-compensated compasses application as well? When checking the datasheet, Tilt-compensated compasses is mentioned only in the 'Applications' of LSM303 and not in ISM303.
I was looking to ISM303 for a Tilt-compensated compass application. Can you please share your comments?
Thanks
Akshay