cancel
Showing results for 
Search instead for 
Did you mean: 

LSM303AGR, Accelerometer Read Address cannot be auto-incremented.

Min-Kyoung Kim
Associate III

​

Hi, I'm using LSM303AGR.

​

I cannot read acceleromter 6bytes from 0x28 _ 0x2D.

It is read only 0x28 register 6 times.

​

I tried to read other register, 0x20 0x21, etc...

​

Likewise, It is read only first address register 6 times or several times.

I also checked MS bit (bit1). it is 1 of course.

BUT!

It works Magnetometer same way!

I can read 6 registers magnetometer data.

Below Configure values.

  1. ODR : 1001 (1.344kHz)
  2. LPen : normal mode
  3. Zen, Yen, Zen : 1
  4. BDU : 0
  5. BLE : 0
  6. FS : 10 (8g)
  7. HR : 1
  8. ST : 00
  9. SPI_ENABLE : 1 (3 wire)

Below, my configuration code and reading code

	Sensor_IO_SPI_CS_Enable(&SensorHandle[ACCEL]);
	valueTx = 0x29;	//8g(Sensitivity : 3.9 mG/LSB), HR mode, 3 wire
	Sensor_IO_SPI_Write(&SensorHandle[ACCEL],LSM303AGR_ACC_CTRL_REG4,&valueTx,1);
	Sensor_IO_SPI_CS_Disable(&SensorHandle[ACCEL]);
 
	Sensor_IO_SPI_CS_Enable(&SensorHandle[ACCEL]);
	valueTx = 0x97;  //1.344kHz, no power down(12bit, divisor : 16), x,y,z enabled
	Sensor_IO_SPI_Write(&SensorHandle[ACCEL],LSM303AGR_ACC_CTRL_REG1,&valueTx,1);
	Sensor_IO_SPI_CS_Disable(&SensorHandle[ACCEL]);
	Sensor_IO_SPI_CS_Enable(ctx);
        Sensor_IO_SPI_Read(ctx,ctx->RegRX, raw_data_tmp.u8bit,6);
        Sensor_IO_SPI_CS_Disable(ctx);

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Eleon BORLINI
ST Employee

Hi, the configuration should be ok, and magnetometer and accelerometer SPI communication should behave in the same way. Also in case of the magnetometer the MS bit is =1? Is it possible for you to share the oscilloscope pattern?

View solution in original post

3 REPLIES 3
Eleon BORLINI
ST Employee

Hi, the configuration should be ok, and magnetometer and accelerometer SPI communication should behave in the same way. Also in case of the magnetometer the MS bit is =1? Is it possible for you to share the oscilloscope pattern?

I didn't know that the acceleromter ​register address is 7 bits.

I didn't set the MS bit to =1.

When I compared MS bit between accel and mag, I got it thank for your comment.

Thank you.

​you're welcome