cancel
Showing results for 
Search instead for 
Did you mean: 

STSW-MKI109W problem with software Unideo-GUI Ver 1.5.2.6906

davidle.ee9
Associate II

Please help:

I had STSW-MKI109W with STEVAL-MKI196V1

Not Recognize the board on Windows 10

Device manager shown:

What is the driver for my Windows 10

Thanks

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Eleon BORLINI
ST Employee

Hi davidle, if your are using STSW-MKI109W you shuold use the associated tool Unico-GUI (at this link, sw version 8.0.0), not the Unicleo-GUI (which I guess you are using since the version number). The associated hardware tool for Unico-GUI is the STEVAL-MKI109V3, with the standard DIL24 socket for your STEVAL-MKI196V1 (LSM6DSO sensor). There should be no issue with win10 drivers.

Btw, if you want to use Unicleo-GUI, you should associate it to the X-NUCLEO-IKS01A2 expansion board hardware.

Regards

davidle.ee9
Associate II

Must hold the BT2 and plug the USB cable to the PC to update FW

Then Use New Unico Version 8.0.0

It works!!!

Eleon BORLINI
ST Employee

​Good!