2015-08-25 4:12 AM
Hi,
I working with Barometric Pressure sensor LPS331AP.Its working good. but as this chip absoluted,then we changed design to LPS25HB.But this chip is reading 6.4mBar error apart from the actual measured value .We are not added any offset value and not done any our factory calibration.Just I reading the 24-bit data and displaing converted pressure.I did 't change any code,just I replaced LPS331AP by LPS25HB chip.Advice me is it nesassary to change any code ? or any calibration or offset vaules need to set?/Please advice us...2015-09-01 3:16 AM
Hi,
the LPS331AP and LPS25HB sensors have a similar register map, but they are not same. I suggest to check the initial setting. You can find attached the datasheet for both devices. Do you have soldered the device on your customized board? If the device is reporting a value with a small offset compared to the expected one, a single point calibration may be needed in order to compensate the post soldering package stress.Regards
AntonellaHi,
I working with Barometric Pressure sensor LPS331AP.Its working good. but as this chip absoluted,then we changed design to LPS25HB.But this chip is reading 6.4mBar error apart from the actual measured value .We are not added any offset value and not done any our factory calibration.Just I reading the 24-bit data and displaing converted pressure.I did 't change any code,just I replaced LPS331AP by LPS25HB chip. Advice me is it nesassary to change any code ? or any calibration or offset vaules need to set?/ Please advice us... ________________ Attachments : DM00036196_LPS331AP.pdf : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HyrL&d=%2Fa%2F0X0000000bJt%2F_dBBD_D1seLR5MeZE4G1yGbpYTTeDIFVXpPI_FQD8q8&asPdf=falseDM00141379_LPS25HB.pdf : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HzJ1&d=%2Fa%2F0X0000000bJp%2FeAoB1wUGNlozK6yuaH7bJB8lasKjhGFlKyt.GoaWQoE&asPdf=false2017-02-15 12:04 AM
Hi~
I am experiencing exactly same problem. I also see 6mbar offset.
Did you find any solution for this problem?
Thanks in advance.
Yeonsik
2017-02-17 4:47 PM
Please check the answer on