2024-09-10 6:52 PM - edited 2024-09-10 11:51 PM
Hi,
I want to compensate for the temperature of the LPS22DF sensor.
how does one go about programming for it?
Is this formula correct?
Pcorrected=Pmeasured−(TCF×(Tmeasured−Treference))
If it is, should I use a temperature reference value of 25°C?
Also, can you tell me the value of the Temperature Compensation Factor?
Can I make a correction formula with TCO(Temperature coefficient offset) with a data sheet and program it?
If possible, please let me know the formula that I can use TCO
Thank you