2024-11-20 07:56 AM
I would like to change the state of the INT_DRDY of LPS22DF. I have tried to change the value of INT_H_L bit in register CTRL_REG3 (12h), but it has no (immediate) effect. Is it necessary to activate the pin? I have also tried different values in CTRL_REG4 (13h), without effect.
Thank you.
Solved! Go to Solution.
2024-11-20 08:51 AM
Sorry, I just found the INT_EN_I3C bit in IF_CTRL (0Eh).
2024-11-20 08:51 AM
Sorry, I just found the INT_EN_I3C bit in IF_CTRL (0Eh).