2019-05-17 12:07 PM
Hi,
I'm using LSM330DLC on my board and I've configured low power mode (accelerometer enters the low power mode in case of inactivity, and goes back to normal mode if I touch/shake it). What I would like to know - if there is any way to know that accelerometer entered the low power mode? In that case I would like to put gyro and MCU into sleep mode and wake up on the interrupt from accelometer.
2019-05-17 12:12 PM
Also, maybe it's possible to configure the accelerometer to produce interrupt on when it enters the low power mode/normal mode?
2019-06-14 5:49 AM
Hi, sorry for our delay in the answer. There are some possible way to know the devices entered the low power mode: the current consumption is low, the output data are on 8bit instead of 12bit. However, I suggest you to use the “Sleep-to-wake�? and “Return to sleep�? feature: the I1_AOI1 in CTRL_REG3_A (22h) should go high after the event detection (that exceeds e.g. ACT_THS) and you can detect it by polling that register or physically route it on INT1 pad. Regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.