2019-10-31 1:22 AM
Hi,
We notice that LIS3DH accelerometer has multiple mode which can be utilized to be used on low power mode for single/double tap detection.
Does single/double tap detection increase the current consumption stated on the data sheet/design tip?
https://www.st.com/resource/en/datasheet/lis3dh.pdf
Thank You
Solved! Go to Solution.
2019-11-25 3:06 AM
Hi @Dillah , sorry for my delayed answer. From the LIS3DH app note AN3308 (p. 31), the recommended accelerometer ODR for single and double-click recognition is 400 Hz or higher. You can however try to lower this ODR and check if the feature is working in your specific application case, if the low current consumption is a major request. Or you could try with a more recent sensor like the LIS2DW12 to get lower power consumption on double tap application. Regards
2019-11-04 7:25 AM
Hi @Dillah , the typical current consumption contribution of a digital embedded feature such as the single/double tap detection (that includes a couple of threshold comparisons) is less than 1uA, a fraction of the overall standard current consumption. Regards
2019-11-04 8:04 PM
HI Borlini,
Thanks for the information.
Is there any recommendation on minimum data rates for acceptable double tap performance?
Noted that tap threshold will be acquired by manual testing on the unit.
We want to use as low current consumption as possible.
2019-11-25 3:06 AM
Hi @Dillah , sorry for my delayed answer. From the LIS3DH app note AN3308 (p. 31), the recommended accelerometer ODR for single and double-click recognition is 400 Hz or higher. You can however try to lower this ODR and check if the feature is working in your specific application case, if the low current consumption is a major request. Or you could try with a more recent sensor like the LIS2DW12 to get lower power consumption on double tap application. Regards
2020-01-28 1:24 AM
Hi @Eleon BORLINI .
Currently we are working in 3V environment, and we are computing power budget.
However we can not find LIS2DW12 averaged current consumption on 3V voltage supply.
I would ask if you have similar data to current consumption vs voltage supply?
Thanks
2020-01-28 2:04 AM
Hi @Dillah , supposing Vdd=vddIO=3V , HPM ODR 400Hz and Low Noise Enabled, the current consumption can reach 300uA. To better this current consumption and still be able to well detect single and double tap recognition, you could try to work in HPM, ODR = 200 Hz, Low Noise Enabled, and should be able to go below 180uA. Which is your power budget?
Note that the current consumption is strictly related to the ODR almost linearly. Regards
2020-01-29 12:31 AM
Hi @Eleon BORLINI ,
Thank you for those information.
Our power budget on accelerometer is around 3uA in 3V supply voltage.
After some evaluation, we will try to use 25Hz or 50Hz ODR as shown on below image.I would ask if you have similar data of current consumption in 3V power supply for highlighted mode?
Thanks
2020-01-29 1:49 AM
@Dillah, of course going in LPM will help the power budget requirements. The curr cons for 3V in LP1 at that ODRs is about 2.5uA with ODR 25Hz, so this is the condition in your case. Please note that the resolution lowers from 14-bit to 12-bit, you should have to check if you can detect the single/double tap in a good way. Regards
2020-01-29 1:57 AM
HI @Eleon BORLINI ,
Thanks for the info.
We will try to test the double/single tap sensitivity of said setting.
2024-02-12 9:27 AM
Hi @Dillah,
Did you have the opportunity to test the current consumption putting the sensor in low power mode?
If so, what was the averaged result?
Reading from the datasheet I'm afraid that sensing single/double tap is only possible running the sensor in high performance mode.
Thanks in advance,