cancel
Showing results for 
Search instead for 
Did you mean: 

[LIS3DH] In High-resolution mode (12-bit data output), why the BW is ODR/9

Kefei Yao
Associate III
Posted on April 03, 2018 at 09:47

In Low-power mode and Normal mode, the BW is equal to ODR/2 which is understandable. But in HR mode, the BW is ODR/9, why?

0690X0000060AI1QAM.png
3 REPLIES 3
Miroslav BATEK
ST Employee
Posted on April 04, 2018 at 17:39

For high resolution, there is a filter inside the sensor which decrease the BW.

Kefei Yao
Associate III
Posted on April 08, 2018 at 07:17

Thanks for the reply. To make sure, the filter you mentioned is only applicable for high resolution mode, thus is a totally different filter than the High-Pass filter which is common for all modes, right? 

Posted on April 09, 2018 at 09:42

Yes, you are right.