cancel
Showing results for 
Search instead for 
Did you mean: 

LIS3DH: How can we reprogram the registers and make it work in a different configuration without power cycling the IC ? Is there any way to reset the IC through software ?

SPoch.1
Associate
 
1 ACCEPTED SOLUTION

Accepted Solutions
TSand.1
Associate III

Hi, you can in general write a different value in a register you want to re-configure, without switching off and on the sensor. Or you can write the default value (usually 00h) in the register. Don't know if I have answered to your question.

View solution in original post

2 REPLIES 2
TSand.1
Associate III

Hi, you can in general write a different value in a register you want to re-configure, without switching off and on the sensor. Or you can write the default value (usually 00h) in the register. Don't know if I have answered to your question.

Eleon BORLINI
ST Employee

Hi @SPoch.1​ , @TSand.1​  is right, check also this similar thread.

-Eleon