2016-10-11 12:34 PM
The datasheet specifies that it has 16 bit output data, but the data that i get out of the registers are 12 bit ie first 4 bits of High Byte is always 0. Am i doing something wrong here or is the effective resolution only 12 bit ?
#lis331 #lis331hh2016-10-12 01:37 AM
You are right, the effective resolution is 12 bits.
The 12 bits resolution cover the measurement range with define the sensitivity (see Table 3 in the datasheet).
For example: FS=+-6g, 2^12=4096 * 3mg/digit (sensitivity) = 12288 = +-6144 mg
Best regards
Miroslav