2020-06-18 12:16 AM
hello.
I have a question about LIS331DLH.
under low temperature, LIS331DLH chip z-axis shows wrong value.
it is almost 100 difference between -10 degree and 22 degree.
x,y axis is fine but only z axis is problem.
every chip I got have same problem except one chip.
is there ways to figure out this problem ?
Solved! Go to Solution.
2020-06-22 09:35 AM
Hi @kdok .1 , in LIS331DLH device the z axis is in effect mechanically "asymmetrical" with respect to the other axis, and this partially can cause a higher temperature dependency (100 LSB in 30°C range, right?). Btw, I would suggest you to check a couple of things:
Regards
2020-06-22 09:35 AM
Hi @kdok .1 , in LIS331DLH device the z axis is in effect mechanically "asymmetrical" with respect to the other axis, and this partially can cause a higher temperature dependency (100 LSB in 30°C range, right?). Btw, I would suggest you to check a couple of things:
Regards
2020-07-15 04:42 PM
Thank you for answer.
I want angle values by using this chip.
I tried to remove DC component. then all DC component value gone with the angle values.