2024-01-11 4:29 AM - last edited on 2024-01-11 7:05 AM by Peter BENSCH
Hi there,
The LIS2MDL Application Note (AN5069) states that the min and max values for each axis needed to run the self-test can be found in the datasheet. However, there is no information in the datasheet.
The application note of the LIS3MDL, on the other hand, provides all values.
Could someone please advise which values to use for the self-test of the LIS2MDL?
Best regards