2024-07-22 11:17 AM
I have configured the activity/inactivity function, but I only get the interrupt raised on inactivity, not on activity. Is this function supposed to be able to alert me to both activity and inactivity? Or is it just inactivity that raises the interrupt?
Solved! Go to Solution.
2024-07-23 6:58 AM
Hi @cchristie ,
Welcome to ST Community!
Yes, only the inactivity raises the interrupt (it is bit INT1_INACT, Inactivity interrupt on INT1).
2024-07-23 6:58 AM
Hi @cchristie ,
Welcome to ST Community!
Yes, only the inactivity raises the interrupt (it is bit INT1_INACT, Inactivity interrupt on INT1).