cancel
Showing results for 
Search instead for 
Did you mean: 

LIS2HH12 activity/inactivity interrupt behavior

cchristie
Associate

I have configured the activity/inactivity function, but I only get the interrupt raised on inactivity, not on activity. Is this function supposed to be able to alert me to both activity and inactivity? Or is it just inactivity that raises the interrupt?

1 ACCEPTED SOLUTION

Accepted Solutions
Federica Bossi
ST Employee

Hi @cchristie ,

Welcome to ST Community!

Yes, only the inactivity raises the interrupt (it is bit INT1_INACT, Inactivity interrupt on INT1).

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Federica Bossi
ST Employee

Hi @cchristie ,

Welcome to ST Community!

Yes, only the inactivity raises the interrupt (it is bit INT1_INACT, Inactivity interrupt on INT1).

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.