cancel
Showing results for 
Search instead for 
Did you mean: 

LIS2DH12 output x,y and z

jan n
Associate II
Posted on October 20, 2017 at 10:46

Hello all, 

my problem is the output of the x,y and z registers.

The content of the registers change when moving, but only with fast movement. The values change during the acceleration. Unfortunately, after the movement the values fall back to the same value again.  The problem is, the values are the same in any orientation. My program accepts different values for x, y and z register in different positions, but the sensor doesn’t change these values. When the sensor is horizontal I accept g_z = 1, g_x = 0, g_y = 0  and when I turn it by 90 degrees I estimate g_z = 0,

g_y = 1, g_x = 0

at least the values should be different. However the values are the same.

Maybe I made some mistakes in the register settings or the sensor is not able to do this?????

My register settings:

Address                                             value

0x1f                                                    0xc0=     1100 0000 // edit: revised

0x20                                                   0x77=     0111 0111

0x23                                                   0x80=     1000 0000

0x24                                                   0x70=     0111 0000

0x2e                                                   0x80=     1000 0000

This discussion is locked. Please start a new topic to ask your question.
8 REPLIES 8
Miroslav BATEK
ST Employee
Posted on October 20, 2017 at 11:17

The configuration seems to be correct, I think the problem will be in your reading procedure. Please check that you red both low and high part of the output registers.  I would recommend you to start read the data without using FIFO, because it is little bit more complex.

Note: 0xC0 = 1100 0000

Posted on October 20, 2017 at 15:00

Hello Miroslav,

i changed the sensor to non-FIFO mode, but the values are still the same in any direction.

Here is how I convert the data from the register to mg:

uint8_t hight;

uint8_t low;

int16_t result;

double result1;

low = readvalue(0x28);

hight = readvalue(0x29);

result = ((hight<<8) | low) >> 6; // convert to 10 bit 

if(result & 1<<9){

result |= (1<<15)|(1<<14)|(1<<13)|(1<<12)|(1<<11)|(1<<10); //convert 10 bit in 16 bit two's complement

}

result1 = result*4 / 1024.0; // *4 because 2g mode, 1024 because of 10 bit

Posted on October 20, 2017 at 15:30

The conversion is not correct (i.e. result = ((hight<<8) | low) >> 6; you rotate the high byte in 8 bit variable).

Use following commands, it will also manage the two's complement format.

result = ((int16_t)high<<8)+(uint16_t)low;

result = result>>6; // in case of normal mode = 10bit output

result1 = result * 4; // LSB to mg (FS=2g), see sensitivity in datasheet

Posted on October 20, 2017 at 16:13

Okay, thank you!

Now I have other values, but the basic values in the registers still not changing.

Do you have another idea??

Posted on October 23, 2017 at 11:06

I guess you are not reading all the output values and because the BDU is enable the data are not updated. You can try to disable BDU, to confirm this theory

You can also share the complete code so I can look at it.

Posted on October 24, 2017 at 08:26

Okay, 

Here is how I set the sensor:

sensor::sensor(char i){

char I2C_ADDR = i;

vector <string> a;

a.push_back('i2cset -y 0 0x19 0x24 0x00');

a.push_back('i2cset -y 0 0x19 0x2e 0x00');

a.push_back('i2cset -y 0 0x19 0x1f 0xc0');

a.push_back('i2cset -y 0 0x19 0x23 0x00');

a.push_back('i2cset -y 0 0x19 0x20 0x57');

a.push_back('i2cset -y 0 0x19 0x30 0x00');

for(auto tmp : a)

   system(tmp.c_str());

this->fd = open('/dev/i2c-0', O_RDWR);

if (fd < 0) {

   cout << 'Error opening file: ' <<endl;

}

if (ioctl(fd, I2C_SLAVE, I2C_ADDR) < 0) {

   cout << 'ioctl error: ' <<endl;

}

}

Here is how I read the sensor(&sharpinclude <linux/i2c-dev.h>):

char sensor::readvalue(char hex){

   char arr = hex;

   write(fd, &arr ,1);

   read(fd, &arr, 1);

   return arr;

}

and here is how I print out the values:

I only show one axis, because they are all alike.

int8_t hight;

uint8_t low;

int16_t ergebnis;

   cout <<endl;

   low = readvalue(0x28);

   cout << hex << +low << ' ';

   hight = readvalue(0x29);

   cout << hex << +hight << ' ';

   cout << '\t\t' << 'achse x: ';

   ergebnis = ((int16_t)hight<<8)+(uint16_t)low;

   ergebnis = ergebnis>>6;

   ergebnis = ergebnis * 4;

   cout << dec << ergebnis << ' ';
Posted on October 24, 2017 at 12:32

Does the value change if the BDU is disabled?

Unfortunately I'm not expect on linux programming so I can't help you with that, but the sensor configuration is correct, it will measure acceleration at 100Hz.

Posted on October 24, 2017 at 13:07

Unfortunately not

:((

.

Maybe i have the wrong sensor. Today I tried a mpu6050 and it gives me the right value of x and y angle. Also the values changing in different positions, but I have to do it with theLIS2DH

Thanks anyway!