2022-01-18 8:08 PM
Hello,
May I get some document information for parts marking of PN#LIS2DE12TR?
The label mark say is A2L 2D? Is it right? Have any document for the marking?
Thanks
Solved! Go to Solution.
2022-01-20 12:28 AM
Only a small amount of information can be put on the small housing of the LIS2DE12. So only the first line containing the date code is legible to the human eye, format: YWW, the code underneath is internal and cannot be read with a QR code reader.
The marking is only mentioned on the label of the packaging unit and has the correct value A2L 2D.
Regards
/Peter
2022-01-19 10:22 PM
2022-01-20 12:28 AM
Only a small amount of information can be put on the small housing of the LIS2DE12. So only the first line containing the date code is legible to the human eye, format: YWW, the code underneath is internal and cannot be read with a QR code reader.
The marking is only mentioned on the label of the packaging unit and has the correct value A2L 2D.
Regards
/Peter
2022-01-20 12:31 AM
Thanks Peter.