Skip to main content
Associate III
June 28, 2024
Question

LIS2D12

  • June 28, 2024
  • 27 replies
  • 4743 views

I use LIS2DS12 

This is my init function

 

 

 

void LIS2DS12_Init(void)
{
	uint8_t ctrl_1 = 0x72; //0111 for 6.4kHz ODR [7:4], 00 for 2g [3:2], 1 for high frequency available[1], 0 for BDU not activated [0]
	uint8_t ctrl_2; // [6] for soft_reset, [1] for disable I2C, [0] for 4 wires SPI
	HAL_StatusTypeDef ret;

	ret = spi_read_LIS2DS12(CTRL2_ADDR, &ctrl_2);
	ctrl_2 |= 0x42; // [6] for soft_reset, [1] = 1 for disable I2C, [0] = 0 for 4 wires SPI
	ret = spi_write_LIS2DS12(CTRL2_ADDR, &ctrl_2);

	//reset the accelerometer
	ret = spi_write_LIS2DS12(CTRL1_ADDR, &ctrl_1);

	//set the accelerometer to measurement mode


	spi_read_LIS2DS12(CTRL1_ADDR, &ctrl_1);
	spi_read_LIS2DS12(CTRL2_ADDR, &ctrl_2);
}

 

 

 

with read and write : 

 

 

 

HAL_StatusTypeDef spi_write_LIS2DS12(uint8_t regAddr, uint8_t *pData)
{
	HAL_StatusTypeDef ret;
	uint8_t address = regAddr & 0x7F;

	uint8_t sendData[2] = {address, *pData};
	HAL_GPIO_WritePin(GPIOB, GPIO_PIN_4, 0);

	ret = HAL_SPI_Transmit(&hspi2, sendData, 2, 20);
	HAL_GPIO_WritePin(GPIOB, GPIO_PIN_4, 1);

	return ret;
}
HAL_StatusTypeDef spi_read_LIS2DS12(uint8_t regAddr, uint8_t *pData)
{
	HAL_StatusTypeDef ret;
	uint8_t address = regAddr | 0x80;

	uint8_t sendData[2] = {address, 0};
	uint8_t receiveData[2] = {0};

	HAL_GPIO_WritePin(GPIOB, GPIO_PIN_4, 0);

	ret = HAL_SPI_TransmitReceive(&hspi2, sendData, receiveData, 2, 50);
	HAL_GPIO_WritePin(GPIOB, GPIO_PIN_4, 1);

	*pData = receiveData[1];

	return ret;
}

 

 

 

The protocol for SPI transmission is 

fru999_0-1719563774185.png

fru999_1-1719563790647.png

But my Register always equal to 0. ret = HAL_OK.

I don't understand why :)

Can you help me

 

This topic has been closed for replies.

27 replies

fru999Author
Associate III
July 18, 2024

and the problem is the same if my datasize is 8 or 16 

AScha.3
Super User
July 18, 2024

Again: did you set data size to 16b ?

here:

AScha3_0-1721318217862.png

+ your data in software also 16b , but: command/send is only in upper 8b , resonse/receive is only in lower 8b of the 16b words.

If you feel a post has answered your question, please click on " Best Answer ".
fru999Author
Associate III
July 19, 2024

this what i get when i analyse my signals :

fru999_0-1721380512644.png

when the thing I am supposed to send is {10001111, 0}

 

 not So the first clock tick is not supposed to be here because the count of clock rise is 17 when it supposed to be 16

fru999Author
Associate III
July 18, 2024

when i use the function transmitreceive i set the size data to 2 bytes

fru999Author
Associate III
July 19, 2024

Yes

The problem remains the same