cancel
Showing results for 
Search instead for 
Did you mean: 

Library/function to acquire QVAR data from the sensor LSM6DSV16X

ECiot.1
Associate II

Hi, I would like to know if there are a library and a function to acquire QVAR data from the ST sensor LSM6DSV16X as for example it is present for the ILPS22QS sensor for Arduino using a Nucleo-64 stm32 board.

1 REPLY 1
Federica Bossi
ST Employee

Hi @ECiot.1​,

There isn't a library only for Qvar sensor but you can refer to the Application Note AN5755.

In section 4.2, there is the register configuration for LSM6DSV16X to enable the Qvar sensor and how to read the results.


_legacyfs_online_stmicro_images_0693W00000bjSX6QAM.pngIf my reply answered your question, please click on Select as Best at the bottom of this post. This will help other users with the same issue to find the answer faster

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.