Is there a way to connect the BlueNRG GUI to the BlueNRG-MS on the SensorTile?
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2019-01-15 3:05 PM
I am developing an application based on the STM32L476 on the SensorTile. I need to be able to configure the BlueNRG-MS chip on the board. To test it, I tried connecting BlueNRG GUI to the SensorTile with and without a Nucleo64 board but was unable to establish that connection.
Is there a wat to connect the BlueNRG GUI to the BlueNRG-MS chip on the SensorTile ?
Labels:
- Labels:
-
STM32L4 Series
0 REPLIES 0