2019-02-04 12:09 AM
2019-02-04 12:21 AM
Your question is not comprehensible.
2019-02-04 12:27 AM
Are the pins of the acceleration and gyroscope sensors compatible? So do you have the integrated model with the same pin structure? i need this problem a solutions. Thank you.
2019-02-04 01:42 AM
Ask ST FAEs or distributors diectly.
Volunteers on a public forum will usually not do the simple due diligence tasks you can easily do yourself.
2019-02-05 02:29 AM
I suggest you to use 6 axis modules which contains both axl and gyro. MEMS gyroscopes are rarely sold standalone.
2019-02-05 02:54 AM
thank you sir.