2024-08-07 09:31 PM
Hello,
I am working on integrating IMP23ABSU into my hardware. Hence, I reviewed the evaluation schematic (steval-stwinkt1b) to understand its setup. I have a few questions regarding the schematic, in addition to what has been answered here, it would be great if you could answer them.
1. There are three MREF in the schematic for steval-stwinkt1b, part of which is attached to this message as an image below. I understand what the ones circled in green correspond to, but what does the MREF circled in red correspond to?
2. In the response here, it was mentioned that the amplification factor of 1 + R6/R7 = 2.34 is to take advantage of the microcontroller's 3.3V. But isn't the Opamp's VCC+ and microcontroller's VREF+ tied to 2.7V? Meaning the analog voltage range will be from 0 to 2.7V and the output M1P can only range from 0 to 2.7V, am I correct in interpreting the setup?
Thank you.