cancel
Showing results for 
Search instead for 
Did you mean: 

IIS3DWB XYZ accel operation in I2C mode and thresholds for wake up and activity interrupts.

JLee.75
Associate II

In I2C mode for the IIS3DWB device the datasheet says it only support single axis mode because I2C is too slow to get the data. I want to use I2C mode to configure either wake up or activity thresholds for all 3 axis and then configure the interrupts to tell me those thresholds were exceeded. I don't need the data.

So the question are In I2C mode:

  1. Are all the axes still active?
  2. Can I access all the registers in I2C mode to configure the thresholds for all axes of the device for the interrupts?
  3. Can I effectively get two thresholds for each axis if I use one set of thresholds for wake up configured on INT1 pin and another set of thresholds for activity configured on INT2 pin?

Regards,

Jeff Lee

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0