cancel
Showing results for 
Search instead for 
Did you mean: 

IIS3DWB - Missing details in datasheet?

TResell
Associate II

When configuring function routing on INT1/INT2 register (MD1_CFG/MD2_CFG), there is a note that says; "Activity/Inactivity interrupt mode (sleep change or sleep status) depends on the SLEEP_STATUS_ON_INT bit in SLOPE_EN (56h) register.

But the SLOPE_EN register only have one bit in the driver library which is "SLOPE_FDS". Where is the SLEEP_STATUS_ON_INT bit?

1 REPLY 1
Eleon BORLINI
ST Employee

Hi @TResell​ , you are right. I internally checked and basically the SLEEP_STATUS_ON_INT is the bit5 of SLOPE_EN (56h) register. This is the bit value:

  • bit 5 SLEEP_STATUS_ON_INT: Sends to INT pads the sleep status instead of sleep change (only if INT1_SLEEP_CHANGE or INT2_SLEEP_CHANGE bit are enabled).

Please check if it is working

Regards