cancel
Showing results for 
Search instead for 
Did you mean: 

I want to use two wake up inrterrupts at the same time. Thresholds and duration will be different. I cannot use it at the same time because I changed the register value while doing the settings.

Iakgu.1
Associate III

I want to use wake up interrupt for two different thresholds at the same time,

for example I want to give wake up threshold 1g for interrupt 1,

I want to give 500 mg for interrupt 2. And duration will be different.

I change the value of WAKE_UP_THS, WAKE_UP_DUR registers while configuring second interrupt.

Is it possible to do it ? How can I do it ?

1 REPLY 1
Eleon BORLINI
ST Employee

Hi @Iakgu.1​ ,

with a bit delay... is this question related to this other thread?

If so, can we close this one?

-Eleon