2020-10-05 05:23 AM
2020-10-05 06:25 AM
Hi, You may need to run the installer (executable file) as administrator.
2020-10-05 06:45 AM
Thanks for the fast answer. I run the SW as administrator on both devices.
Does the SW works on every Windows System? I try it with Windows 10 (64 bit).
Regards
2020-10-09 07:35 AM
Hi @DPalm.1 ,
I'm afraid that STSW-IMG004 is so far a NRND product...
VL53L1X st.com Tools&Softwares page shows a lot of possible GUIs for the device interface.
For example, you can use the STSW-IMG008 pack which looks as the evolution of STSW-IMG004.
-Eleon
2020-10-09 08:15 AM
You are absolutely right Eleon. The STSW-IMG004 is the GUI for VL6180X device. If you want to evaluate the VL53L1X device you need to install the STSW-IMG008. And you have to install with the Administrator right. Anyway I don't understand why you couldn't install the STSM-IMG004 on your computer ?