2021-04-06 11:36 PM
I have LSM6DSO sensor. I want to use fsm. In application note, I did not understand how thresh1 is calculated . For example it is written that
B7AEh (-0.480)
3C00h (1.000)
27AEh (0.030)
34CDh (0.300)
I did not understand how this conversion is done.
Solved! Go to Solution.
2021-04-07 4:41 AM
Hi @Iakgu.1 ,
As described in the AN5226 application note, the unit of measurement of the 16-bits thresholds is that of the selected signal:
So, it basically depends on the selected sensor, and on the settings of that sensor.
Consider the In the example, the threshold case 3C00h (1.000) g, i.e. the wake-up threshold is 1.0 g ± 30 mg. Suppose you are using the accelerometer, configured with FS = +-2g: the calculation is the following:
3C00h (LSB) --> two's decimal conversion --> (decimal)--> times sensitivity (0.61 mg/LSB, see datasheet p. 9) --> 0.9375 g
Probably it is a little different from 1g since it is taking into account some residual offset or some margin for a more effective recognition of the threshold in that specific finite state machine example...
-Eleon
2021-04-07 4:41 AM
Hi @Iakgu.1 ,
As described in the AN5226 application note, the unit of measurement of the 16-bits thresholds is that of the selected signal:
So, it basically depends on the selected sensor, and on the settings of that sensor.
Consider the In the example, the threshold case 3C00h (1.000) g, i.e. the wake-up threshold is 1.0 g ± 30 mg. Suppose you are using the accelerometer, configured with FS = +-2g: the calculation is the following:
3C00h (LSB) --> two's decimal conversion --> (decimal)--> times sensitivity (0.61 mg/LSB, see datasheet p. 9) --> 0.9375 g
Probably it is a little different from 1g since it is taking into account some residual offset or some margin for a more effective recognition of the threshold in that specific finite state machine example...
-Eleon