MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Allowed values for interrupt threshold of LIS2DH12

Hi, I am using a LIS2DH12 chip to detect the orientation(in 3D space) of a device.For this purpose I'm using the INT pins in 6D position mode to generate interrupt signal/s, that will alert me if the device has exited/entered a known positional area....

ilg by Associate
  • 1965 Views
  • 2 replies
  • 0 kudos

Resolved! High-pass path: BW_FILT setting

When BW_FILT[1:0] = 00, it's different between AN5201 AND DATASHEET. Which one is real?​in AN5201:In Datasheet(DocID031788):​​

0693W00000FBx7wQAD.png 0693W00000FBx8BQAT.png
user1 by Associate
  • 1118 Views
  • 1 replies
  • 0 kudos

Resolved! Unable to initialize X-CUBE-MEMS1 libraries

I'm using a NUCLEO-L476RG with a STEVAL-MKI197V1, connected in SPI mode without any expansion board. My setup works: I successfully used the LSM6DSOX low-level driver to read sensor data. But my attempts to use the high level libraries, such as Motio...

paul19 by Associate III
  • 3540 Views
  • 6 replies
  • 0 kudos

Resolved! IIS3DWB static and dynamic noise question

Hello ST team, I’m using the IIS3DWB (STEVAL-MKI208V1K) together with an Arduino Portenta H7. No filter added through the composite group of digital filters, only the default LPF1. Also, 2g scale resolution.When placing the sensor on a surface isolat...

FCook.1 by Associate III
  • 3206 Views
  • 2 replies
  • 0 kudos

Resolved! Sensor Fusion output parameters.

Could you recomend me a document that speaks about the format of the matrix parameters obtained trought sensor fusion? For example: linear_acel, quaternion... Best regards.

RBAGU.1 by Associate II
  • 1685 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.