cancel
Showing results for 
Search instead for 
Did you mean: 

I am using the example project MEMSMIC1 in order to stream audio to host PC. But it is not working beside the following configuration: 2 channels, 16000 sample rate.

AA.10
Associate III

When I am changing the number of channels to 1 channel.

it is recognized by the windows driver, but the

"advanced" TAB is disappear (unlike 2 channels configuration). 

Did someone faced with this kind problem? Do I missed

something? 

of course, audacity do not allow to record and I receive this message:

" error while opening sound device"

10 REPLIES 10

It works! Thank you so much!​