When I built the project with 192000 sampling rate(which is the sampling rate used when first time I build the project and connect it to PC), the Advanced tab shows.I saw another post: https://community.st.com/s/question/0D50X00009XkgUySAJ/xnucleocca...
That is exactly what we do. The problem is: the Advanced tab is not there, if we set other sampling rates (except 192KHz in my situation) in the project and build and run.
I have similar problem with Nucleo-L476RG and MEMSMIC1 5.4.0 package. In 48KHz, the Advanced tab is gone and Audacity or other recorders failed to start recording. Also on Win 10. Any solution now?Update: The only sampling rate that works on my mach...