2020-01-27 5:58 PM
I am already able to build firmware, which blinks LEDs, but I would like to cut some corners.
2020-01-28 3:41 AM
Hi @AKuru.1 , you can find STEVAL-MKI109V3 .ioc file here.
If you just want to interface LSM9DS1 and STEVAL-MKI109V3 in a custom way, it is not difficult to start a new project on STEVAL-MKI109V3 from scratch: you can base on STM32CubeIDE and create a project for STM32F401VE MCU and enabling the appropriate interfaces as described by the STEVAL-MKI109V3 schematic.
If you want to control the Unico GUI, I suggest you to download the Unico lite source code, which enables you to modify part of the interface.
Regards
2020-01-28 10:52 AM
I was looking for this: https://github.com/STMicroelectronics/STMems_Standard_C_drivers/blob/master/_prj_MKI109V3/_prj_MKI109V3.ioc
Thanks.