2023-09-26 12:57 AM
I set the CTRL1_XL (10h) of ISM330ISN as 0xA4 ,so the ODR of ISM330 is 6667Hz.
If I want transmit the whole data @6667Hz to external RS485 ,How tocontroll it ?
Can I Using the ISM330 INT1 to trigger every transaction ? or independently transmit data using timer of
STM32L431CCT6?
2023-09-26 8:04 AM
Hi @JohnGe ,
Welcome to ST Community!
I would suggest to send more data with a single communication, so the best way would be to use the FIFO, save a certain number of data and then send every data with a single UART communication. As an easier version, you could also try to use the normal interrupt and use a custom FIFO inside your code where you store all the data and then send it in a single comm every once in a while.
If this helps you, please mark my answer as "Best Answer" by clicking on the "Accept as Solution" button, this can be helpful for Community users to find this solution faster.