2020-07-09 04:57 AM
What I have:
What I already did:
What is my goal?
Problem:
Questions:
What would be the more future proof path? Adapting the AWS-cloud example or using X-CUBE-CELLULAR as base framework?
Thanks for your help and best regards
Patrick
Solved! Go to Solution.
2021-03-25 07:02 AM
Hi @Eleon BORLINI
I am using STSW-STWINCELL demo application on STEVAL-STWINKT1B with STEVAL-STMODLTE, most of the time I keep getting this error but once in a while it works fine, it connects and sends the topics to AWS.
Can you please help me fix this issue?
SIM which I am using work perfectly fine on my phone, so there is no connection issue.
Kind Regards
Chandrashekar C
2021-03-26 09:04 AM
Hi @Chandrashekar C ,
I checked with our experts and they say that it is unfortunately an issue related to the server chosen for the synchronization with the TLS protocol.
In fact the cellular module is perfectly connected to the net as shown in your picture, with his own IP address.
They suggest the following procedure:
Please let me know if you can fix the issue in this way.
-Eleon
2021-03-26 11:39 AM
Hi @Eleon BORLINI
Thanks for the response.
I followed the procedure you suggested in the above message, its still same, I doesn't connect at all :( not even once.
Do you think it's anything do with setting Tickless to 1 to achieve Low power mode?
#define configUSE_TICKLESS_IDLE 1
Please let me know if I can tweak in anything else.
Kind Regards
Chandrashekar C
2021-03-26 01:01 PM
Hi @Eleon BORLINI
I also notice that the binary provided in STSW-STWINCELL [STSW-STWINCELL_BG96_V1.0.0.bin] also behaves same [ RTC failure ]
Is there any other working binary which I can use?
I am using SIM card from onomondo
Any suggestion is much appreciated.
Kind Regards
Chandrashekar C
2021-03-30 03:11 AM
Hi @Chandrashekar C ,
Our experts performed some tests (described here below) without encountering issues. The outcome is that your issue could be related to supply problems.
Test configuration:
HW
FW
Please find attached the log files.
The modem obtains the IP address and can configure RTC from both www.gandi.net and www.st.com.
Their suggestion is:
-Eleon
2021-03-31 07:42 AM
Hi @Eleon BORLINI
Thank you so much for your detailed response and patience.
Looks like there is an issue with network provider, Onomondo SIM on specific network fails to connect to www.gandi.net or www.st.com.
Currently, we are whitelisting selected network and it seems to be working 🙂
Further, I have couple of question for you
Looking forward for your response.
Kind Regards
Chandrashekar C
2021-04-01 03:10 AM
Hi @Chandrashekar C ,
glad to hear that you solved your previous issue!
About the new questions, could you write them in a new community post, so that people can interact with it you more easily?
-Eleon
2021-04-01 10:57 AM
Hi @Eleon BORLINI
Thanks.
Sure, I will create a new community post with these questions.
Kind regards
Chandrashekar C