cancel
Showing results for 
Search instead for 
Did you mean: 

How to use my own board with Unico-GUI

CLI.2455
Associate

I used the breakout and evaluation board with Unico.

Now I want to use my own board with sensor.

I want to use Unico to capture, process, display sensor data.

I may need to implement the communication protocol via serial port.

Do you have some documents about how to do it? Thanks

1 REPLY 1
Eleon BORLINI
ST Employee

Hi @CLI.2455​ , not so simple to interface a custom board with Unico-GUI... you should at least use the same MCU of the to STEVAL-MKI109V3 and a similar schematic in order to be able to upload the proper firmware (which is however not open) and make the Unico-GUI compatible with the hardware platform. Regards