2024-08-29 1:47 PM
Hi All
I am running Unicon GUI on Windows 10 and using it to communicate with STHS34PF80 sensor plugged onto STEVAL-MKI109V dev board.
I can fully interact with the senor via the GUI app. Meaning reading and writing all registers of interest.
I however want see what registers are being written and read by the GUI so I attached my logic analyzer to the I2C pins but unable to read any sensible data. So I am assuming that the motherboard is communicating over SPI.
I want to be able to sniff the interaction between the GUI app and the senor over I2C.
So what do I have to do to make the GUI change communication protocol.
Ola
Solved! Go to Solution.
2024-08-30 2:32 AM
Hi @ola ,
You can change the communication protocol in the Comm. & Power Settings tool window:
2024-08-30 2:32 AM
Hi @ola ,
You can change the communication protocol in the Comm. & Power Settings tool window:
2024-09-04 9:53 AM
Hi Federica,
Thank you for your reply. Unfortunately I can see the page that you are showing on my version see below.
Regards
Ola
2024-09-04 9:56 AM
Correction:
Unfortunately I can not see the page that you are showing on my version of Unico-GUI.
Regards
Ola
2024-09-04 10:50 AM
Hi Federica,
Looking at your image again. I noticed that you were using MEMS-Studio which is meant to have replaced the old Unico-GUI application that I was using.
I have downloaded the MEMS-Studio and I can now read the I2C bus correctly. Thank you.
Regards
Ola