cancel
Showing results for 
Search instead for 
Did you mean: 

How to resolve a STM32CubeProgrammer error: "Error: No STM32 target found!" while using a ST-Link/V2-lsol probe connected to a SensorTile.box eval board via the 20->14 pin adapter?

dmcph.1
Associate

I have a SensorTile.box eval board connected to a ST-Link/V2-lsol using the 20->14 pin adapter. The ST-Link/V2 is connected to my linux workstation via USB and the ST-Link is seen by the STM32CubeProgrammer application. The SensorTile.box is also connected via its micro-USB port to provide power. The SensorTile is up and running and I can connect from my mobile phone with the ST BLE Sensor app to read the sensor data and I see the blue LED flashing to indicate a valid bluetooth connection. However when I try to connect to the eval board from the STM32CubeProgrammer I get a popup with the message: "Error: No STM32 target found!". Any ideas or suggestions on what the problem is and how to fix will be greatly appreciated.

1 REPLY 1
dmcph.1
Associate

here is a screen capture of my STM32CubeProgrammer GUI:

0693W00000WJsrUQAT.png