cancel
Showing results for 
Search instead for 
Did you mean: 

How to give power supply to the IMU sensor ASM330LHB

Deviprasad Bokkisam
Associate II

The IMU sensor is  working on two input voltage supply 1.Vdd - Core supply 2.Vddio - digital I/O supply.My questions are in below.

1.Is it better to supply the Vdd and Vddio seperately from two voltage regulators? 

2.Is it better to supply the Vdd and Vddio from single voltage regulator?

3.Which method 1 or 2 is best, to increase the accuracy of IMU sensor?

4.What are power supply specifications(Ex: Output voltage accuracy and PSRR-power supply rejection ratio etc)?

1 REPLY 1
Federica Bossi
ST Employee

Hi @Deviprasad Bokkisam ,

About 1-2 question there is no difference to supply the vdd and vddio with one or two different voltage regulator if they are at the same voltage.

About question 3: method 1 or two doesn't change the accuracy of IMU sensor.

For the power supply specifications you can refer to the datasheet.

However, we do not provide PSRR values as it is only tested in characterization and is not guaranteed in production.

 

 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.