cancel
Showing results for 
Search instead for 
Did you mean: 

How to design a High Speed data logger?

Khairul Akmal Zulkepli
Associate II
Posted on June 04, 2018 at 15:13

Hai, I want to build a data logger attached to an object travel at 3m/s. The requirement is the data logger must capture 74 sensor input (10 bit ADC) at every 3mm along the travel path. Thus in 1 second, the data logger must capture and save 3000 data per sensor and equivalent to 222 000 data for the whole 74 sensors.

I never exposed to this task before thus could you give an idea of the architecture of such system?.

#store-data #high-speed
0 REPLIES 0