2012-08-30 04:40 PM
Hi,
in the example code of the LPR430AL there are written these values in the Header. one is from datasheet but where is the other from ? LSB/dps ? Where can i get my LSB value?/*!<300dps Full Scale Pitch axis Sensitivity [ mV/dps ]see LPR430AL datasheet*/ #define Gyro_Sensitivity_P_300dps 3.33
/*!<300dps Full Scale Pitch axis Sensitivity [ LSB/dps ]*/ #define Gyro_SensitivityLSB_P_300dps 4.13 I need the LSB Value to calculate the Densivity for the LPR45AL. Please Help WR Ersan #lpr450al-gyro-lsb-value-stm322012-08-30 07:33 PM
Hi Ersan,
Gyro_Sensitivity_P_300dps = 3.33STM32F103 microcontroller's 12-bit ADC is used to digitize Gyro signal.
Gyro_SensitivityLSB_P_300dps = (212 -1) / (300*3.3)
Gyro_SensitivityLSB_P_300dps = 4.13
4.13 is the sensitivity of 4x amplified output.Now, sensitivity when not amplified is :Gyro_SensitivityLSB_R_1200dps = 4.13/4 = 1.0325Hari