cancel
Showing results for 
Search instead for 
Did you mean: 

How to calculate LIS331HH wakeup threshold

Hello All,

I try to set threshold of INT1 in LIS331HH
According to the datasheet the sensitivity of the sensor can be set to(3 , 6 , 12)mg/digit
And the threshold register is 7-bit register


Can anyone confirm these calculations or there's another factor must be added to set the threshold :
Threshold(mg) = (Sensitivity) * (7-bit value)

For ex :
To set threshold to 1g . and set the sensitivity to 12mg/digit :
1000 mg = (12) * register value
register value = 1000/12 = 83

 

0 REPLIES 0