cancel
Showing results for 
Search instead for 
Did you mean: 

How do you install PDM library ?

EEnco.1
Associate III

I struggle to use PDM Filter library.

This is the message error I get :

0693W00000KbhBQQAZ.pngWhat I have done so far are : - in project properties, C/C++ general, Paths and syombols, in "Includes" I added the path to pdm2pcm_glo.h ; in "Library Paths" I added the path to a folder with all the libPDM_FIlter_CM3_GCC_wc16.A ... files.- Wrote #include "pdm2pcm_glo.h" in the main.

It's still not working :\

In "Paths and Symbols", in libraries, I think I can add a library but I don't know which one to use (all the files were included in mems1 folder). I tried randomly picking but I had another error message;

0693W00000KbhEyQAJ.pngI am new to cubeIDE so it's very possible Im doing a beginner mistake here

10 REPLIES 10
FShah.1
Associate II

Thanks @ghrairim the problem has solved.